Example Programs and Installation Folders
Example Programs
                                            
 Most example programs listed in this help, as well as many other code samples, are available at http://www.keysight.com/find/iosuite. Code examples are only for Windows at this time. 
IO Libraries Suite Installation Folders
See the appropriate section below for Windows 
 or Linux. 
Windows
Click the Keysight IO Control 
 and select About Keysight IO Libraries Suite to see the specific installation directories used on your PC, as shown below.
                                            
                                        
Linux
In Linux, IO Libraries suite is installed at: /opt/keysight/iolibs